Part Number: LV14340
Tool/software:

Hi,
I am using this circuit to convert 12VDC to 5VDC. Due to some mistake with the footprint we were unable to mount the D13 diode (Part : SK54-3G) on the PCB directly, so for the prototype we soldered one end of the diode directly to the capacitor and a 1 inch jumper wire from other end to a ground point.
I have verified that the connection is secure and not touching any other components.
The issue is sometimes the output voltage just drops after a few seconds, it keeps on fluctuating. Other times, it works fine with 5V output and the rest of the board working fine.
I want to ask if the wire length added can cause such an issue, I just want to make sure there are no other issues before I go for the redesign.
Although it is not clear from here but I can confirm that C32, D13, L4 and U4.8 are connected.