This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: IT Algorithm, Coulomb counter

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO

Tool/software:

Hello.
We are designing drone batteries using BQ40Z50-R2.
In some cases, drones use more than 40A when using Sense Resistor as 1mohm, and in this case, I wonder if it is applied to IT algorithms.
Max values for Gas Gauging - State - Avg I Last Run and Avg P Last Run are 32.768A and 327.67Wh respectively. If so, I was wondering if bq40z50-r2 can't be used for drones using 40A or if it's applicable to IT algorithms up to 100A since it's -0.1V to 0.1V, which is the input voltage spec for Coulomb counter.