Tool/software:
Dear Sir/Madam,
I am currently using a LM25116 to recieve voltage from an automtoive main battery (8V to 32V) and outptut a 5V supply (3 Amp max current).
The circuit works fine in our intended 8V to 32V input range. What we have noticed is that for input voltages below 8V the LM25116 will output voltages below 5V. This has an undesired effect that some downstream devices turn off before others.

When aproximatley 5.7V is applied the undervoltage lockout (UVLO) of the LM25116 kicks in and turns off the 5V output.
My question is: How can I ensure that the LM25116 still ouptuts at least 4.6V even with lower supply voltages? Alternatively is there a way to completely kill the output voltage from the LM25116 at supply voltages below 8V ? I still need to ensure that the LM25116 outputs 5V when 8V-32V is applied to the LM25116.
Below is my schemaitc.

Note:
I was trying to improve thte UVLO performance of the LM25116. Using 0.1% 34.8 kOhm and 6.55 kOhm resistors but this still results in a worst case turn turn off voltage of 6.74V.
Any suggestions would be greatfully recieved.