This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751: What EU standard could TPS25751 pass

Part Number: TPS25751
Other Parts Discussed in Thread: TPS26750, TPS65987DDK

Tool/software:

Hi Team,

Could you please give us a list about the Type-C+PD standard we can pass regarding our PD controller? such as TPS25751.

Could it pass  IEC 62680-1-2(USB PD) and IEC62680-1-3(C Function)?

Thank you,

Yishan Chen

  • Hi Yishan, 

    TPS25751 supports the current IEC 62680 standards and meets PD3.1 specification. Our current portfolio for PD3.1 solutions are shown below:

    • TPS25751 (TID 10306 and 11449) - DRP PD controller supporting up to 100W (20V/5A) for battery charging applications, includes PPS and liquid detection. No Alt mode support
    • TPS26750 (TID 11450) - similar to TPS25751 but supports EPR (Extended Power Range) up to 240W (48V/5A). No Alt mode support
    • TPS65987DDK (TID 7766) - DRP PD controller supporting up to 100W (20V/5A) for NB, docks, monitors. Supports Alt mode such as DisplayPort and Thunderbolt. 

    Let us know if you have any further questions or concerns! 

    Thanks and Regards,

    Raymond Lin