Tool/software:
Hello.
The UCC28064A is continuously operated in single-phase mode to operate the PFC circuit.
Look at the waveforms [ch1: FET_Vds, ch2: IL, ch3: FET_Vgs, ch4: VCin].
This shows the waveform at startup, where the falling edge of the coil current waveform is not straight.(waveform1) In addition, the triangular waveform is extremely small.(waveform2) When these occur, the voltage waveform of Cin behind the diode bridge is disturbed. Only at startup is such an unusual waveform seen. The current capacitance of the X capacitor and the Cin is 2μF. This is the limit of the capacitance size because the board layout makes it impossible to increase the size. Also, the coil is not saturated.
Are there any other countermeasure suggestions besides changing the constants of the capacitor and coil?
Does the waveform disturbance at startup cause any abnormality in normal operation?
Thanks.