Tool/software:
Hello, We're seeing MCU (STM32L151RET6) resets and traced it back to 1.8V rail dropouts happening on the TPS63030DSKR output. It appears that this may be happening during the transition out of PS mode (see images). These dips are causing sporadic resets on the MCU and we're not sure how to address. The design has been in production for quite some time and we're still getting data on whether any other components have been substituted in the overall design, but it doesn't look like it. This issue has only recently been detected, but again, we're still investigating other avenues such as firmware changes, etc.
What I would like to request is confirmation that this output dip is normal behavior at the PS mode transitions. It appears to be possible based on Figure 20 in the datasheet, but that graph is for PS mode disabled and for a load transient. I suspect that there may be some sort of MCU activity that causes the regulator to exit PS mode, but no proof of that yet.
Another solution that came to mind is permanently turning off PS mode via firmware, but this is going to increase current draw significantly I think. Am I interpreting Figure 8 correctly that the quiescent current draw is several mA when not in PS mode? Our sleep current is only 50uA so we cannot afford mA of extra current draw in our battery application if that is correct.
Final solution would be to adjust the regulator voltage to 1.9V to increase the headroom for the MCU but obviously that is a hardware change so, not as desirable.
Thank you for your help,
Clifton Lin