This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750: -300V 200mA power supply on Webench

Part Number: UCC28750


Tool/software:

I am trying to design a -300V 250mA supply (off line, with isolation). The WEBENCH tool only allows for up to -80V, and it allows for up to 1000V positive supplies. What is the reason for this discrepancy?

I felt that, for a flyback converter,  changing the  polarity of input, and the output diode would give a equivalent negative supply. Or, can I design it as 2 rails 1, positive and other negative. with feedback being taken from the positive supply? 

Thanks,

Sasi

  • I cannot explain why Webench shows this discrepancy. I can route your inquiry to them if you prefer.

    Since the primary and the secondary are isolated, the polarity of the Vout just depends on where your ground definition.