This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: The change of RM between new battery and aged battery

Part Number: BQ27426

Tool/software:

Hi TI teams

根据TI的资料,我们了解到RM = (DODfinal - DODpresent) * Qmax,而在充放电过程中,DODpresent = DOD0 + PassedCharge/Qmax。

那么,如果我同时给一个老化的电池和一个新电池放出相同的电量,电量计如何确保两者的RM变化量保持一致呢?

我认为,由于老化电池的DODfinal和Qmax都会减少,这将导致计算得到的RM变化量增大。

如果在上面场景下,电量计输出的RM变化量确实不一样的话,那RM和实际放出的电量之间的关系是什么?

According to TI, RM = (DODfinal - DODpresent) * Qmax, and during charge and discharge, DODpresent = DOD0 + PassedCharge/Qmax.

So, if I discharge the same amount of power to an aged battery and a new battery at the same time, how can the fuel gauge ensure that the RM change of the two batteries is consistent?

I think that since the DODfinal and Qmax of the aged battery will decrease, this will cause the calculated RM change to increase.

If the RM change output by the fuel gauge is indeed different in the above scenario, what is the relationship between RM and the actual amount of power discharged?