This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: two LEDs in series vs. single LED short

Part Number: TPS929120-Q1

Tool/software:

Hello TI Team,

My custoemr is using 2 LEDs in series at each TPS929120 channel with 7.5V constant voltage supply.

They need to put device into Fail-safe mode - as it needs to work as standalone without communication.

However, cusotmer requires single-LED-short and LED-open detection in Fail-safe mode.

After looking at datasheet Table 7-4 I understand single-LED-open will work in Fail-safe mode.

What about single-LED-short in such application? Is there a way to make it working in Fail-safe mode?