Part Number: TPS2117
Tool/software:
Please confirm if there is any problem with the circuit. I have not connected ST to our platform for the time being
In addition, since we also need to be compatible with manual MODE, I would like to confirm how to connect the mode pin in manual mode
The partial pressure of PR1 is 100K- 75K
The default voltage is up to 4.35V
Minimum 3.3V
According to your specification, the manual mode is compared with PR1 and Vref (1V)
When VIN1 and VIN2 are both greater than 1.6V, PR1≥Vref is VIN1 output and < is VIN2 output