Other Parts Discussed in Thread: LM70660, LM5148, LM5085, LM5137
Tool/software:
Hey Buck Regulator Team,
I have a customer evaluating the LM706A0 for a new design and we are running into an error when trying to generate and simulate a design based on the following input/output conditions:
- Input range: 42V - 57.4V
- Output: 24V at 10A
The error mentions that the design is not stable due to the phase margin. Can you please help to provide guidance as to whether or not this device can support the given application or if there is an issue with the WEBENCH model?
If there is another device in your portfolio which would be better suited for these power conditions we are open to your suggestions as well.
Best regards,
Matt Calvo