This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A74: TPS7A74

Part Number: TPS7A74

Tool/software:

Hi Team,

I am using the TPS7A7401DSDR part for Vin=1.8V & Vout=1V with Bias Voltage of 3.3V, Iload=1A

While checking for the drop out voltage, the condition fails for my case. so what would be the required drop out voltage for Vbias=3.3V

from the graph i could see the drop out voltage value for the Vbias=5V condition, i need to know whether i can use for my requirement.

the below graph shows the drop out voltage more than 750mv, which is not possible for my Vin, Vout range.

the graph values shows 750V in the Y-axis, is it a typing mistake?