Hi,
I would like to ask a question on bq27x00 connection.

Question 1
I could not understand the "Typical Application" schematics in bq27x00 datasheet. In the right upper corner of the schematics, the current should come out of the positive end of the battery, and after flowing through components of the system, eventually come back to the negative end of the battery through the GND network.
If this is the path of the current, then why would current through sense resistor RS? It seems that no current would flow between GND and PACK- at all.
I guess the GND network in the right upper corner might be wrong. Could anyone confirm it?
Question 2
What does the Li-ion Protector stand for? Does it refer to circuit/temperature circuit in the battery pack?
Zheng