This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76905: OCD1 threshold program

Part Number: BQ76905
Other Parts Discussed in Thread: BQSTUDIO, BQ76907EVM, BQ76907

Tool/software:

Hi Expert,

The OCD1 in discharge is -4mV ~ -200mV in datasheet. The default is 68mV, so the max current is 68A. In my test, when the current is 10A, the OCD1 is triggered and the FET disable accordingly. You can see below waveform of current test.  In fact, the load current will achieve 50A in a while.

  1. How to program the OCD1 to higher threshold? Which is register should be configured in BQStudio GUI?
  2. Whether the default OCD1 value is 68mV? or 10mV?