This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
On the datasheet for the TPS6306x parts, I can't seem to find a specification for the voltage threshold levels on the device enable (EN) pin. It just references "high" / "low" or "1" / "0". This is being controlled with a microcontroller, so EN can't be tied directly to the input.
What is the minimum voltage required for 1, and what is the maximum voltage required for 0?
Thanks