Tool/software:
LED照明用としてドラバTPS92200の採用を検討しております。
入力電圧は12VでLEDの順方向電圧10.2Vとなります。電流は350mA流します。PWMの調光制御は行いません。100%のまま固定で使用します。
この場合、入力電圧とLEDの出力電圧の差が12V-10.2V=1.8Vとなるのですが、入力と出力間の電圧が1.8Vと小さいのですが、LEDを点灯させることはできるのでしょうか。
定格順方向電圧10.2V,350mAのLEDを駆動させるために必要な、最低入力電圧を教えてください。