Other Parts Discussed in Thread: LM5156
Tool/software:
Hi TI experts,
With LM5022 isolated flyback design, i have a few questions:
1. There is an internal 1.4V offset at COMP pin, but datasheet 7.3.5 mentions :"The PWM comparator polarity is such that 0 V on the COMP pin results in a zero duty cycle at the controller output.". Is this true? 0V at COMP means -1.4V divided by 3 at internal PWM generator.
2. What is the desired COMP voltage variation range for isolated flyback design? Is Duty cycle proportional to COMP voltage?
3. COMP is internally pulled up to 5V through a 5kohm resistor. What's the current limitation of internal 5V reference?
4. As FB is grounded in isolated flyback design, Is there any additional bias/leakage current which drawn from 5V reference? or any additional current source to opto Ic current?
Thanks
Neo