Other Parts Discussed in Thread: BQ25758, TPS25751, TPS25730
Tool/software:
Hi TI,
We are designing single cell battery chargers and there will be a total of 20 battery charging ICs in parallel with 0.5A output. We would like to use simple battery charging ICs with 5V input and without any programming involved. Pleas note that our input if coming from PD charger. We are thinking to just use a 5V, 10A Buck-Boost regulator with input coming from USB-C PD. I would like to know if can use BQ25758S only as a 5V, 10A output and if yes then please help me to understand this chip before going with it please help me to answer these questions so that we may proceed accordingly. If BQ25758S can't be used as a Buck-boost only then please suggest an alternative PD compatible regulator;
1. I can see this BQ25758S is a Buck-Boost converter with Charger features as well and this is confusing me to think if we can use it only as a 5V output and without using battery charging feature. Please confirm.
2. I have a quick look on this BQ25758S datasheet stating that the default output is 5V. Can you please confirm that we can safely use it to generate a 5V, 10A output? As per the datasheet equation (4) is showing how to set the max current limit. I am assuming that if we will use the 5mOhm then we may set the max current output limit to 10A. Please confirm?
3. Any recommendation for the PD chip to use along with BQ25758S. As you know our application is USB PD sink only.
4. BQ25758S is not where available. Can you please confirm on its availability and time. I can see BQ25758 that is in stock that has even wider input range and I believe both are pin compatible.
Kind regards,
Muhammad Awais