Other Parts Discussed in Thread: LM5060
Tool/software:
Hi Team,
In practical applications, customers recently discovered that three LM5060 circuits were damaged. Two of them had burn-through marks near pin 2, and one had burn-through marks near pins 8, 9, and 10. The circuit schematic is as follows, and the power supply input voltage It is 24V and the rated current is 100mA. Please help to check if there is a problem with the customer's principle design? Thanks.