This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51772: Schematic review

Part Number: LM51772
Other Parts Discussed in Thread: LM5177

Tool/software:

Hi Team,

Please assist with schematic review schematic review.

Vin 9~36V,Output: 12V/12A

Not using I2C

Thanks

  • Hi Allen,

    thank you for using the E2E forum.

    Could you please attach the filled out LM51772 Design Calculator to this thread? This would be the most efficient workflow for us to do a schematic review.
     

    Best regards,

     Stefan

  • 嗨斯特凡,

    請注意CFG1~4、nRST、VIN-FB、VIN-FB。
    此設定有任何問題。
    請告訴我如何糾正它。

    目前有Buck功能,沒有Boost功能。

    謝謝

  • Hi Stefan,

    Soft reminder.

    Do you have any comments on the schematic? Thanks.

    Regards,

    Terry

  • Hi Stfan,

    Modify schematic:

    C3514, R3519, R3520 Remove

    nRST to Vin,

    CGF2 R3509 short to GND

  • Hi Allen Hi Terry,

    the schematic image is very hard to read esp. the pins of the LM51772 are not read able.

    To your last comment first:

    C3514, R3519, R3520 Remove : OK

    nRST to Vin, : required

    Please see below my review list and bold marked line items which should be checked again (Note: other info are left here to give an overview of what has been checked)

    Checked with Quickstart Calculator

    • Slope compensation should be set to 1.5 see line 36 -> R_CFG1 = 8.3k
    • Inductor de-rate could be set to 20% -> R_CFG3 = 2.7k
    • Cross over frequency is much to high -> recommend is 28k
    • Phase margin too low : should be > 60 Degree
      (note: check over full Vin range)
    • Losses seems quite high - check if this is OK with thermal disipation

     Schematic:

    • Rcs in series with inductor and before inductor
    • Check filter for Rcs
      Current sense Resistor Rcs does not have the required filter
    • Check filter for Risns
      Current sense Resistor Risns does not have the filter - recommend to add place holder
    • Connect IMONOUT to VCC if ISNS not used
      Connect ILIMCOMP  to VCC2 if ISNS not used
    • Snubber on SW1 and SW2
      Place Footprint for a snubber at SW1 and SW2
       (they can then be populated in case needed (e.g. due to EMI) without layout change)
      Note: Snubber connect Resistor to GND for better Thermal performance
    • BIAS connected
      If BIAS is not used connect to GND or VIN of VOUT (do not keep open)
      BIAS can be connected to VIN (if the max ratings of BIAS are not violated) to benefit from the better performance of the LDO on BIAS
    • Add Series Resistor into MOSFET Gate signals lines
      (they can then be replaced in case needed (e.g. due to EMI) without layout change,
      additional option: add a diode in parallel for slow on and fast off.
      Note: Good starting value is 2.2Ω and then adjust in when testing out the PCB
    • Voltage rating of MOSFET
      (Have a margin of 30% is recommended)
    • Miller Plateau of MOSFETs
      used MOSFETs need to be logic level MOSFETs - can be seen by Miller Plateau in the range of 2.5V-3.5V
      Do not recommend to use this MOSFETs
    • UVLO setting relative to lowest input voltage
      UVLO is set to xV but operating range starts at xV - relative large distance
    • Cap at VCC 22uF : (Datasheet min: 6uF with DC Bias)
      please check the cap on Vcc to have the required capacitance considering DC BIAS - we use a 22uF on the EVM
    • VCC2 is for control and driver supply
      VCC1 can used for external logic - if not used can be disabled
    • Feedback divider identical for FB and FBIN (check if FBIN is required)
    • FB_IN required: for pass through mode - only with external FB divider. With internal FB (FB connected to VCC2) put this to AGND
    • LM51772: Connect FB to VCC2 if voltage should be set via I2C
    • nRST if not used needs to be connected to VIN

     

     

    For layout guidelines the layout please have a look at this application report first: https://www.ti.com/lit/pdf/slvafj3

    Best regards,

     Stefan

  • 1. 如果未使用 ISNS,則將 IMONOUT 連接到 VCC

         ==> IMONOUT = 腳位?

    2. MOSFET 的米勒高原

        ISC027N10NM6 米勒高原=4.5V,可以嗎?

    3.CFG2設定0ohm可以嗎?

       不使用PCM

    4.CFG4設定1.9k歐姆可以嗎?

      負電流限制&電流限制,感應ISNS還是CS?

    5. PCM未使用設定

        CFG2設定0歐姆

        VIN-FB 至 GND

     

  • Hi Allen,

    1. Yes,

    2. Miller plateau to high for the LM5177

    3. yes 

    4. Negative Current limit & Current Limit which could selected here is related to ISNS

    5. Yes

    Not sure which file is the Schematic and if there is any question on it.

    Best regards,

     Stefan

  • 1. IMONOUT = Pin 10 CDC ???

    2. CFG2 VDET_EN  is control register or hardware Pin?

  • Hi Allen,

    not sure what the question are but let me try:

    1. the current monitor (measure of the voltage proportional to the current measured at ISNS) can be measured at the CDC pin 

    2. VDET_EN can be enabled via the CFG2 resistor setting , If enabled the device will only start to operate if VIN is above the VDET_EN level.

    Best regards,

     Stefan

  • Hi Allen,

    the thread got active again but I do not see a reply. In case this got lost please enter it again.

    Best regards,

     Stefan

  • Hi Stefan 

    No doubt

    thank you for your support