Tool/software:
I have been studying the behavior of TPS61236 in detail using the TPS61236EVM. I'm trying to learn something about the margins of stability for the EVM layout and component choices, and I found a few surprising things. First, the datasheet output capacitance spec is 10 uF minimum "effective capacitance". A footnote mentions the negative effects of voltage bias on capacitance, which I was expecting. However, there is not mention of dissipation factor D or frequency effects. I looked closely at the datasheet for the Murata GRM188R60J capacitors in the EVM BOM, and their capacitance is specified at only 120Hz for C>10 uF and 1kHz smaller capacitances. I desoldered and measured capacitance of the 10uF and 22uF caps in the EVM with my PM6304 Analyzer and found that these capacitors are virtually useless above 1 kHz. At 120 Hz, parts are well within spec, but my Analyzer sees them as resistors with a little parallel capacitance at less than 10 kHz. It seems that it's unrealistic to expect much from large value 0805 10V caps at even mid audio frequencies. The EVM schematic uses 3 22uF caps in parallel, with no other capacitors. Is it possible that this converter will be unstable if I install high quality output caps? I will continue my bench investigations. Meanwhile, does anyone from TI have any comment?