Part Number: UCC24624
Tool/software:
The input transformer is fed with an AC signal of 264V at 30kHz +/- 12kHz ( NOT LLC). Previously we were using half bridge diode rectification to get the output voltage of 48V.Now We want to modify the circuit having 48V output to synchronous rectification.The load power is 9KW. Can i use UCC24626 as it is not LLC. If yes then what should be the implementation step.