This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: Application issues.

Expert 2020 points
Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: GPCRB

Tool/software:

Hi Team,

Using BQ40Z50-R2,

The specification book states that there are 0-7 options for the CONSENT CURRENT mode.
Our product will be used in situations where there is a large temperature difference and current variation. Which mode should be selected for CONSENT CURRENT? (It will be at minus 5 degrees and the current will vary greatly from 3A to 13A).