This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: single solution for 24V and 48V battery pack

Part Number: BQ76940
Other Parts Discussed in Thread: BQ76952, BQ76907, BQ34Z100

Tool/software:

I am trying to find a single solution for 24V and 48V battery pack. 

I have considered BQ76940 and BQ76952 for this solution, but combined solution for both type of batteries looks difficult.

BQ76940 supports minimum of 9 cells so 24V solution would not be feasible with single AFE.

BQ76952 supports 3 to 16 cells but would need another solution to short the unused pins for 24V pack.

Would it be a good idea to use stackable solution with 2*24V battery pack =48V and configure to single for 24V where required.

1. Do you have any soutions for above configuration?

2. I would require atleast 5-6 48V packs in parallel to provide the required current, so using same solution for parallel should be possible with replication?

Let me know your feedback, if possible with part number or reference design.

Thanks,