Tool/software:
Hi,
When I do a flashdump using BQ studio 1.3.127 (or 1.3.111) of my BQ76972, the data memory is only read to 0x9327. However, balancing parameters are out of this range as one of those registers is at 0x9342 for example. Is this expected? Or how can I change this range?
Our goal is to be able to simply export using the flashdump and then convert this file with a simple script to a .h file. But if this export isn't complete we have to find another way.
I hope you can help us!
Kind regards, Robert Jan