Tool/software:
The EV2300 automatically disconnects when it reads the Gauge, resulting in no visibility into battery parameters.What could be the reason? my windows is windows11
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The EV2300 automatically disconnects when it reads the Gauge, resulting in no visibility into battery parameters.What could be the reason? my windows is windows11
Hello June,
I see that the device is not being auto-detected. Please ensure that the gauge is properly being powered. Also another thing to check is the gauge could be in shutdown mode, so if you ensure that the gauge is being power then apply a voltage on the PACK pin to wake up the gauge from shutdown.
Regards,
Adrian