Tool/software:
Hello TI Engineers,
I want to change my current schematic (photo is attached below) of the BQ24133 charger circuit to a standalone configuration. I want to remove the power path circuits but still want to keep the reverse blocking FET (Q4a1) in order for the battery voltage in the VCHARGER node. I also do not need the input current limit to the charger. This means I will not be using the Rac (R29). I just want to confirm which components can I remove
1. I will be removing ACfet (Q4a2) since I only need Reverse Protection FET (Q4a1)
2. Since R29 will not be used, what is the connection for ACN and ACP? Is C29 and C30 still needed?
3. Since Input Current Limit will not be used, what is the connection for ACSET?
4. Since there is no power pathing and the 9V Input Power Adapter will just be connected to PVCC, do I only need a single bulk capacitor of value 4.7uF similar to Figure 10-5 in the BQ24133 datasheet?
5. According to the datasheet, for charging currents of 1A, we would need a 6.8uH inductor. If it is between 1A and 2A, what is the recommended value? anything in between 3.3 and 6.8uH?

Thanks,
Deniel