Part Number: LM5148
Other Parts Discussed in Thread: LM5146
Tool/software:
Hi Team
could you provide any recommendation solution for below spec?

please also recommend any mosfet solution or reference design:)
thanks for your help!
BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
For the 12V/8.3A design, take a look at the LM5146 EVM, https://www.ti.com/tool/LM5146-Q1-EVM12V. This EVM is 12V/8A at Fsw = 400kHz using 100V MOSFETs. Note that an 80V controller may be somewhat tight for a 75V max Vin, hence the recommendation for a 100V controller. Another advantage is the LM5146 drives standard-logic FETs.
For the 5V/10A design, you may want to check design circuit #1 in the LM5146 datasheet, which is 5V/12A/3000kHz: https://www.ti.com/lit/ds/symlink/lm5146.pdf#page=36.
Regards,
Tim