Other Parts Discussed in Thread: BQ25883
Tool/software:
Hi, TI expert
We have an enquiry from a customer regarding BQ25886.
Is it possible to distinguish the status of charging and complete charging only by the status pin?
The intention is to read the voltage status of the battery during charging and display the completion indication at an earlier time than the set value.
Is the behaviour after turning on the MCU during charging, rather interfering with the battery charging? I am asking because the full charge indication is too late.
I have set the charging current to 500mA / full charge voltage to 500mA.
Please check if there is a way to read the battery status during charging.
Is it possible to distinguish the status of charging and complete charging only by the status pin?
Thank you.