This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5190-Q1: CC-CV regulator design

Part Number: LM5190-Q1
Other Parts Discussed in Thread: LM5177, LM5190

Tool/software:

Hi everyone,

I just want to make sure that this LM5190-Q1 synchronous buck controller works well for my application, which is to create a circuit with constant current and constant voltage (CC-CV) supply. The prerequisites are:
Vin = 43V to 57V 
Vout = 48V
Iout = 10A