Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ78350, BQ76200, BQ76940,
Tool/software:
FAE, Hello!
I have made a 14S lithium battery protection board using BQ78350-R1+BQ76940+BQ76200. Currently, I have produced 15pcs of samples, but 4pcs of them are NG. The phenomenon is PF-SUV raising the flag. When testing BQ76940 PIN44-ALERT, the voltage changes from 0V to 3.3V every few seconds. However, when reading the voltage of CELL 1-14 from BQ78350, it does not meet the SUV conditions. Can you help me analyze the reason for this? The schematic diagram and test phenomenon diagram are shown below.
Thank you.