Tool/software:
Dear Team,
We are using BQ76952 in our design for 16S configuration.
From the reference manual it is known that to make the AFE to come out of deep sleep one of the options is to connect charger on the PACK+ side which is the load side.
The AFE is out of deep sleep when we connect the charger in Hard start, i.e., when there is Voltage at the charger terminal and charger is already turned on.
The AFE is still in deep sleep when we connect the charger and then turn on the charger, i.e., soft start of the charger.
Is this normal or else any issue with the design?