This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616EVM-021: BQ79616 EVM - UART Programming

Part Number: BQ79616EVM-021
Other Parts Discussed in Thread: USB2ANY, BQ76PL455EVM

Tool/software:

Hello, 

I'm interested in communicate my laptop with the BQ79616EVM board, but designing an script in python using pyserial library. 

So, as far i now, the board is capable of working with the SW GUI given from TI side (BQ AUTOVAL) via USB2ANY or UART port to connect the board with an MCU. Then, here I have 2 questions:

1. Is it possible to use the BQ79616EVM + USB2ANY + Laptop designing my own python script? If possible, may you tell me please, how can I manage the communications? Is any SDK available?

2. Is it possible to communication BQ79616EVM + Laptop vía UART via UART-USB 5V connector (the same cable used in BQ76PL455EVM)? If possible, may you tell me, please, what are the consideration that I have to consider?

Thanks in advance. 

JR