Other Parts Discussed in Thread: LM10010,
Tool/software:
Hi,
I want to evaluate the LM10010EVM but encountered an issue when using the GUI. Following the setup instructions I downloaded both the LM10010_GUI and CDM20600 executable application. In the GUI I also made sure to update the DLL path to the NSC folder which contains the ftdi_vid_library.dll file.
For the setup, I have the EVM powered at 5V from a lab bench power supply. When powered on the EVM defaults to 1V just fine. I Think my GUI is not communicating to the FTD mini module.
However I am getting this error " Call Library Function Node in host_adapter_close.vi->VID Panel30.vi" Attached is a snippet of the GUI and error.
Looking for the solution .Thanks