Tool/software:
Hey,
I was wondering if someone could check over my schematic and layout to see if there are any improvements that may help the operation of the device and/or reduce EMI.
The device is to be used with a 9-36V input, 12V output. Allow up to 10A however the use case is that this feeds multiple switches for inductive loads with will have 5A kick in for <500ms then 1A continuous.
Schematic:
3D:
Top layer:
Inner 1 GND:
Inner 2 GND:
Bottom Layer:
And this is being fed by my input circuit:
How does this all look? ALso, in the EN pin that is driven by my MCU suppossed to be pulled down to PGND or AGND? I have it to AGND currently!
Thank you in advance!