Tool/software:
Hi
I am using TPS16410 to help me guarantee that output power is below 15W. (But I want to be close to 15W.)
Vin (and Vout) is 12V
I have Rplim = 100 kOhm (measured to 100.1 kohm)
And calculate with the below formula that Plim (nominal)= 14.5 W
However, this is not what I measure. Using a DC Electric load and using a current measuring multimeter to confirm current and multiplying with the voltage at the output capacitor of the TPS16410 I consistently get ~15.5W before the eFUSE trigger and block the output, on several units.
Also, I am wondering about the formula above, it does not fully align with the numbers given in the datasheet. Is there a more complicated but correct formula to use? What are the tolerances of this formula?
I would expect that the +-5% mentioned in the spec are related to the nominal value i.e. 13.69 +-5%, but how should I find the nominal value?
And, are there layout considerations that has to be considered to get accurate power measurements?
Best Regards