This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5012: LP5036 operation on one bus

Part Number: LP5012
Other Parts Discussed in Thread: LP5036, , LP5030, LP5018, LP5024, LP5009

Tool/software:

Good day, colleagues,

My customer is currently using 4 pieces of the LP5036 LED driver in a project and would like to add one LP5012 to the I2C bus due to the additional requirements of the LEDs.
I saw that the bus address is 0X3X on the LP5030 and 0x1x on the LP5012. In this sense, all LED drivers would have to be able to be operated on one bus. Can you confirm if it is possible here? Any potential problems on the bus address?

According to the data sheet, I can see that the components are very similar. Is the control of the registers of LP5012 and LP5036 the same, or are there significant differences, and what about the other devices LP5024, LP5009, LP5018?

Thanks,

Daria