Hello,
I was not able to find on tps65590 DS the absolute maximum ratings and electrical characteristics of pins AUXL-R.
Absolute maximum ratings I mean the maximum voltage I can apply without breaking the input.
Thanks
-g
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I was not able to find on tps65590 DS the absolute maximum ratings and electrical characteristics of pins AUXL-R.
Absolute maximum ratings I mean the maximum voltage I can apply without breaking the input.
Thanks
-g
Giovanni,
The absolute maximum voltage on any input is referenced in the data sheet on page 27 as "1.0 * Supply".
As the AUXL and AUXR inputs are referenced to VINTANA2 the maximum voltage would be either 2.5 or 2.75 depending on the setting.
Richard Elmquist
Elmquist, on DS is reported "maximum output voltage": does it work for inputs, too?
I would not recommend going any above than the recommended operation (1.5Vp-p). I do not have the abs max voltage. Why would customer want to stress the AUX input?