This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5036: the schematic review of Power=500W

Part Number: LM5036


Tool/software:

Hi Ti guys

I am now using TM5036 to make a 550W output 

Vin=48V,Vout=24V,Iout=23A

The primary side uses three MOS in parallel, and the secondary side uses two MOS in parallel.
Do LM5036 and UCC21225 have sufficient drive capability?

I am worried that this multi-MOS parallel circuit will lead to increased switching loss of MOS