Tool/software:
Hello!
Can you please help me with more information for the following watchdog chip: TPS3435JFMAFDSER.
I see that this chip has a preset delay of 50s, but I want to scale it and I saw that the scaling could be 1, 2 and 4. I want to scale to 4. I need a minimum delay of 180 s (3 minutes).
Can you please give me more information about how to set the SET0 pin so that I can achieve the scaling factor of 4? What level should I choose for the SET0 pin?
I have another question about the same class of watchdogs, TPS3435, for which I posted below its footprint and pinout:
Do you have a part number for this footprint? It seems that it can be found even on your site, but that would be great for the application I am using. I have a space constraint board and the package that came in is perfect, also could be configurable. Doesn't have an enable but that could be solved with some extra components.
Thanks! I am waiting you answer.