This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51772: Inductor de-rating setting

Part Number: LM51772


Tool/software:

Dear Sirs and Madams,

I would like to know about the inductor derating settings (INC_INDUCT_DE-RATE).

Table 7-6 of the data sheet provides inductor derating settings.

What is the difference in effect between "Disable" and "Enable", and between "30%" and "40%"?

Regards,

Masashi

  • Hi Masashi,

    Thanks for using the e2e forum.
    Our expert for the LM51772 device is out of office today.
    We will into your question and get back to you within 1-2 days.

    Thank you very much for your patience.
    Best regards,
    Niklas

  • Hi Masashi,

    inductor de-rate could be set via I2C on 4 different levels.

    With the R2D interface only two of the available options could be selected:

    30% and 40% (depending if the setting of the INC_IND_DE-RATE in the R2D)

    Best regards,

     Stefan

  • Hello Stefan,

    I don't understand the relationship between the slope compensation equation (29) and INC_INDUC_DERATE in Table 7-6.

    Referencing the example in the datasheet.

    By back-calculating from equation (46), we can see that fsw is 600kHz.

    We also understand that Leff = 2.5uH is the inductance taking saturation into account.

    I don't really understand the relationship between the calculated coefficient of 1.04 and the high coefficient of 1.5 stated in the text.

    Furthermore, from the 24% inductor derating mentioned in the last sentence, we can understand that this is when a 3.3 uH inductor drops to 2.5 uH due to a large current.

    From "settting for 30% derating could be used", I learned that it is good to set a derating of 30% for 24%, but I don't really understand how it relates to the coefficient calculated by MSC.

    Regards,
    Masashi

  • Hi Masashi,

    please have a look at the Table: ADDR/Slope Pin (R2D-CH1) Configuration Overview"

    You will see that the next higher value from 1.05 is 1.5 - as stated in the description from the calculated value you should select the next higher possible value which can be selected -> 1.5

    Due to the inductor de-rate (inductance get less) the inductor ripple current will get higher.
    MSC defines the slope compensation, so a value which will be added to the measured inductor peak current to avoid sub harmonic oscillations.
    Due to the inductor de-rate you get a higher inductor peak current and therefore do not need to add so much slope compensation -> MSC need be selected lower if not using the inductor de-rate setting.

    Best regards,

     Stefan

  • Hello Stefan,

    I was able to understand it thanks to your explanation.

    Regards,

    Masashi