This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: Basics of reading on I2C

Part Number: BQ27426


Tool/software:

Gauge team,

Can you outline the steps involved in reading the Device Type from the Control Register? I thought it would be something like the steps below, but the customer keeps getting 0000.

S 55W A 00 A 00 A 01 NP    <- Write the Standard Command 0x00, Set the Control Subcommand to 0x0001

S 55W A 00 A Sr 55R A 04 A 21 NP <- Read the Control register, Device Type

Where:

55W = AA

55R = AB

Here's what they see (SDA yellow, SCL purple):

Thanks,
Darren