Team,
My customer would like to possibly put 3 of these in parallet to achieve a 6 W solution. Is this a safe option?
As a secondary request, how efficient are these at light loads? Do they have a ECO/pulse skip feature?
Thanks,
Aaron
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
My customer would like to possibly put 3 of these in parallet to achieve a 6 W solution. Is this a safe option?
As a secondary request, how efficient are these at light loads? Do they have a ECO/pulse skip feature?
Thanks,
Aaron
Hi Aaron -
It is possible to connect multiple DCP020505 in parallel to get higher output capacity. The data sheet recommends also using the SYNC feature to eliminate any beat frequency issues that may occur if the oscillators are left to free run.
Regarding the light load efficiency, there is a table in the data sheet that describes the No Load Current for the various family devices. With no load, it can be between 12mA, and 27mA depending on which device is being used.
thanks,
Jake
DCP020505: Miniature, 2W Isolated Unregulated DC/DC Converters
Product Folder: http://www.ti.com/product/dcp020505
The DCx products including the DCP020505U are unregulated converters. They only share when the Vout voltageof one versus output current droops to less the other. . They can share about to 75% of the 2W rating and not more than 2 are recommended in parallel. The output voltege unloaded or about 5mA load can be as high as 11V .
At 75% load( 300mA) on one DCP020505 with exactly 5 Vin(+/-1%) the output voltage is 5V with range of 4.75V to 5.25V.
Tom