This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: Re-Sequence is not storing to RAM

Part Number: UCD9090A
Other Parts Discussed in Thread: UCD9090

Tool/software:

I have been having an issue where it seems like I can't save the re-sequence commands to the UCD9090. For example, I select unlimited re-try's with 104ms in between. When I store this to RAM everything seems good. However when I try to induce a fault for a test, all rails shutdown but it never tries to come back up. So I tried to restart the program and it should read the current config on the UCD9090 when I load back in, however, I look to see that the re-sequence is in 1 try with 0ms between re-try's. My thought is that something is wrong such that what I am trying to do is an invalid configuration. 

Thank you