This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Supply design input range is 9-38VDC , dual outputs 3.3VDC @2A and 5VDC@2A , 2A is minimum requirement , output currents can be more also

Other Parts Discussed in Thread: TPS54240, TPS54383, TPS54283, TPS51220A, TPS40170, TPS40057, LM25119

I am designing a power supply for a communication unit:

Input range : 9-38VDC.

Dual Outputs are required :

a.3.3VDC @ 2A /more - for processor .

b.5VDC @2A/more  - for all the peripherals.

As the processor should be turned ON first , then the peripherals , power sequencing is required.

i.e 3.3VDC is ON first , then only the 5VDC.

Please assist the best solution for the same.

 

Thank you in advance,

 

Best Regards,

 

Sanjay