Tool/software:
Dear Sirs and Madams,
I would like to know about "Table 7-7 CFG4 Pin (R2D-CH4) Configuration Overview" in the LM51772 datasheet.

Even if the current limit is set to "DISABLE" in settings #1 to 8, will the HICCUP mode go into effect when an overcurrent occurs if the HICCUP mode setting is "ENABLE"?

I think disable of the current limit will disable the peak current limit between CSA and CSB.
If the current limit is disabled, what triggers the entry into HICCUP mode?
Regards,
Masashi