Other Parts Discussed in Thread: UCC27223, INA849
Tool/software:
hi
i use tps40090 and ucc27223 make a 4 phase buck controller,because i need constant current control,so i bypass the internal err opamp,use external err opamp and connect the output to tps40090 comp iput directly,and use instrument opamp to acquire each phase inducor current。when powered up ,the pwm signal seems strange,it works as the picture,all 4 phase pwm signal will shutdown few millionsecons and then back to normal。
then i give voltage directly to the comp input, when voltage beyond 1.4v,pwm signal begin(just as i read from the forum),then the duty cycle quickly rise and get into the discountious mode,when voltage beyond 2v,pwm rise to max and didn't shutdown again。
can you give me some guides to figure it out,thanks