This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS922054: Powering 12V LED Strip With 12V input to Driver

Part Number: TPS922054

Tool/software:

Hello,

We are trying to pull 1A through a 12V LED strip. The voltage drop across these LEDs is 11.6V @ 1A.

1. Is it possible to use a 12V supply to power these LEDs while making use of the TPS922054?
2. Looking through the datasheet and forums we have come across a VCC_TH variable (section 8.3.6 of the datasheet). Does VCC_TH = (Vin_min - Vout_max) * R_UVP2 / (R_UVP1 + R_UVP2) > 1.4V? If not what is it?
3. It is also mentioned here https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1288219/faq-how-to-design-the-uvp-resistor-divider-for-tps922055-tps922054-tps922053-tps922052 in Steven Li's answer (number 4) that UVP can be left floating if not used. Does this mean we dont have to worry about the 1.4V? We worry that we will need Vin_min = Vout_max +1.4V.