Tool/software:
hi expert
This is our flyback power supply schematic scheme, input 350V, output 16.5V, transformer parameters, Lp=1.5mH, turn ratio 9:1:1, now we have two problems in debugging:

1.Problem 1: During the startup process, the PWM output of the chip will be off for a period of time (within 5ms);


Problem 2: When the load is light (less than 200mA), the hiccup will be more serious.