Tool/software:
Hello,
I am looking for a RAD-Hard load switch suitable for a 5V rail with a load of 3.2 Amps. The switch must feature a controlled slew rate, an enable pin, and meet radiation hardness specifications of over 60 krad and 40 MeV.
After searching your catalog, I could not find a dedicated load switch but came across an eFuse that appears to fit these requirements. Would it be feasible to use this eFuse as a load switch? Are there any limitations or considerations I should be aware of when doing so?
Additionally, do you offer any load switches that meet the specifications outlined above?
I appreciate your guidance and recommendations.
Best regards,
Ai